NumericFunctions.Extract expression
Use the EXTRACT function to return a date/time field from a datetime or interval.
Format
ANSI-SQL Format:
EXTRACT ( { YEAR | MONTH | DAY | HOUR | MINUTE | SECOND } FROM expression )
ODBC Format:
{{ FN EXTRACT ( { YEAR | MONTH | DAY | HOUR | MINUTE | SECOND } FROM expression ) }}
Remarks
The returned value is a numeric value that reflects the value of the field that is being extracted.
EXTRACT( YEAR FROM CurrentTime )
EXTRACT( YEAR FROM TIMESTAMP \'2025-11-12 10:23:35\' )
EXTRACT( YEAR FROM INTERVAL \'1\' YEAR )